Command/Query
:DISPlay:TRACe{Tr}:Y:SCALe:RLEVel <numeric>
:DISPlay:TRACe{Tr}:Y:SCALe:RLEVel?
This command sets value of y-axis reference line.
|
Description |
Value at Y-axis reference line |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
- |
|
Preset Value |
100 |
|
Unit |
- |
|
Resolution |
- |
{numeric}<newline><^END>
10 OUTPUT 717;":DISP:TRAC1:Y:SCAL:RLEV 0.01"
20 OUTPUT 717;":DISP:TRAC1:Y:SCAL:RLEV?"
30 ENTER 717;A
:DISPlay:TRACe{Tr}:X:SCALe:RLEVel
TDR/TDT > input box under the right knob (Under Vertical)